Tem alguma questão? Precisa de algum material específico? Disponibilizamos comunicados de imprensa atuais e imagens com qualidade de impressão para download.  
ContactoGostaria de pertencer à nossa lista de contactos de imprensa

Comunicados de imprensa por área

iglidur X: Plain bearing material withstands temperatures from -100 to + 250°C06/07/2015

iglidur X is the perfect material for applications that can be really hot, cold or harsh. iglidur has been designed by igus for extremely difficult environments. These include extreme operating temperatures from -100 to +250°C, even in continuous operation and with aggressive chemicals.

iglidur X provides a significantly longer life in practice
The chemical resistance of iglidur X makes it ideal for use in, inter alia, fuel pumps. Traditionally other plain bearings such as PTFE-coated bearings have at times contaminated the fuel and damaged the shafts. Now the iglidur X bearing ensures a longer service life of the pump. One of the most extraordinary areas of application of iglidur X was in the "Porton Man", a robot used for testing protective clothing in the British defence industry. This was among the submissions for the 2015 manus competition for exciting bearings applications. The rugged iglidur X bearings that withstand the stress of chemical, biological or radioactive materials are applied in all joints of the robot being used for testing the protective clothing.