Tem alguma questão? Precisa de algum material específico? Disponibilizamos comunicados de imprensa atuais e imagens com qualidade de impressão para download.  
ContactoGostaria de pertencer à nossa lista de contactos de imprensa

Comunicados de imprensa por área

igus® to present over 100 new products at Hannover Messe Fair07/04/2014

igus will be presenting more than one hundred new products at this year’s Hannover Fair, the direct result of intensive company research and development. The plastics expert will be showcasing a wide range of product line expansions, and exciting world firsts, all in Hall 17 at the Hannover Exhibition Grounds April 7-11.

A wide variety of products on display

At the show, igus will be showing a variety of new products from its dry-tech® range of products for moving applications, all of which will soon be available from stock world-wide. These exciting up-and-coming igus solutions include a new iglide® material; the W360; specifically designed to have an exceptionally long service life in continuous-running applications, as well as good temperature resistance and high wear durability.

Additionally, igus’ popular bar stock will be on display – now available in round rods to virtually double the variety of materials available for custom machined applications. To add iglide’s self-lubricating properties to any surface, a new 0.5 mm thick iglide ‘tribo-tape,’ made from the iglide A160 material has also been developed. The tape, which is FDA compliant, provides freedom of design in the construction of tribologically stresses sliding surfaces.

Perhaps most exciting is the new igus tribo-optimized filament for 3D printers, enhanced with iglide strength and wear-resistance. The filament material is 50 times more resistant to abrasion than standard filament materials, and will allow for quality prototypes and specialized parts to be printed with the same excellent wear and friction properties of iglide plastic bearings. The filament, which will be available to customers shortly after the Hannover Fair, will be available in a standard 1.75 mm thickness, and more sizes will become available over time.

New solutions for cables and cable management

New Chainflex® cables and Energy Chain® cable carriers will be on display for the first time as well, including the new chip tight Energy Chain R2-75 tube. The tube is able to be opened from both the left and right sides for easy installation, and the tube’s special shape gives extreme protection against dust and chips in rough applications.

igus will be putting some of its products to the test live at the show, including an 11.5 foot span of energy chain, suspended in water under very high tensile forces, just as it would experience in offshore applications like drilling ships or oil platforms.

Celebrating unique applications of igus products

As well as unveiling new products at the Hannover Fair, igus will also be honoring the winners of the igus vector Awards. This competition recognizes extraordinary and interesting applications of plastic energy chain systems. The gold, silver, and bronze winners will be awarded from among the nearly 200 applications submitted from 28 countries around the world.