Tem alguma questão? Precisa de algum material específico? Disponibilizamos comunicados de imprensa atuais e imagens com qualidade de impressão para download.  
ContactoGostaria de pertencer à nossa lista de contactos de imprensa

Comunicados de imprensa por área

Harnessing the secrets of nature: the E4Q energy chain from igus wins the German Design Award23/10/2020

After winning a large number of awards in recent years, igus once again proves how progressive design can bring the user concrete benefits. This also applies to the E4Q energy chain. It is striking that igus has taken a new path here. "In order to optimise the material and thus the weight of the energy chain, our developers have been inspired by nature", explains Michael Blaß, head of the e-chain systems division at igus. "The rounded design is very organic and is found on the outside of the chain links and the stop-dogs. This reduces the weight by 10 per cent compared to the previous E4.1 series, and also the drive energy." Despite the material cut-outs, the new development has 20 per cent higher strength and stability. The chain links of this energy chain generation continue to have a completely new crossbar concept with locking straps. These ensure that the series can be opened and closed in seconds without tools. Filling is therefore particularly easy, and the installation time is reduced by 40 per cent.

German Design Award honours innovative design trends

The advantages of the E4Q have now been recognised by the international jury of the German Design Award. In the Excellent Product Design category, the E4Q was awarded as well as the innovative Module Connect Adapter, with which energy chains including cables can be connected to the machine by means of a click system. The German Design Award is the international prize of the German Design Council. Its objective is to discover, present and award prizes for unique design trends. 5,000 products/projects from 60 countries were submitted this year.

Learn More about E4Q here